Now let us try an actual performance analysis.
Here, we describe how to analyze the performance of func1.
|
Set the first line of func1 as the timer start point, and the last line as the timer end point. |
![]()
![]()
![]()
![]()


|
The timer start and end points are set as shown in the figure above. |
When you have finished setting up the timer, run the program, and analyze the performance.
|
Run the program, and break at any point. Next, display the timer measurement on the Event panel. |


|
As shown in the figure above, the results of the timer measurement appear in the Event panel. |