The I/O files of the CcnvCA78K0R are shown below.
| 
 A C source file or C header file for the CA78K0R is input and the converted C source file or C header file for the CC-RL is output. The version information of the CcnvCA78K0R is inserted at the beginning of the converted file as a comment and the former description of the converted code is left as a comment. The extension of the input file is fixed. If a file with another extension is specified, the input file is directly output without its contents being converted. The converted file can be specified with the -o option or -l option. If a converted file is re-input, the file is directly output without being converted, and the fact that the file was already converted is notified.  | 
|||
| 
 Text file which includes the input file names and output file names. Specifying the list file with the -l option enables multiple source files to be converted collectively. For the format of the list file, see "-l option".  | 
|||
| 
 Messages in the conversion result that is output to the standard output file can be output to a file specified by the -r option. For details on the messages, see "MESSAGES".  | 
Examples of an input file and an output file are shown below. For details on conversion specifications, see "CONVERSION SPECIFICATIONS".