This option performs conversion with the -za option (which is an ANSI-compliant option of CA78K0R) enabled.
Conversion is performed with the -za option disabled.
When this option is specified, the following words are not regarded as keywords and they will not be converted.  | 
Specify this option if the -za option is used in the CA78K0R development environment before conversion.  |