The conversion specifications for reserved words are shown here.
| 
 When the -ansi option is specified in the CC-RL, change the _Bool type to the char type.  | 
||
| 
 For details, see "Interrupt handler".  | 
||
| 
 For details, see "Interrupt handler".  | 
||
| 
 For details, see "ASM statements".  | 
||
| 
 For details, see "Interrupt handler for RTOS".  | 
||
| 
 For details, see "Absolute address allocation specification".  | 
||
| 
 The operation rules of the far pointer conform to the CC-RL specifications. For details, see the user's manual of the CC-RL. The location to write the __near or __far keyword in the declaration of a function pointer differs between the CA78K0R and CC-RL. Since the description location is not modified in the CcnvCA78K0R, it has to be modified manually. For details on the description location of keywords, see the user's manuals of the CA78K0R and CC-RL.  |