The output formats of messages are as follows.
 
-  | When the file name and line number are included  | 
 
-  | Message number type is information  | 
 
| 
 
file-name (line-number):message-number:[information-type] message 
 | 
 
The information type is change, insertion, deletion, or information.
 
-  | Message number type is other than information  | 
 
| 
 
file-name (line-number):message-number:message 
 | 
 
 
-  | When the file name and line number are not included  | 
 
 
The message number is output as a consecutive string consisting of one alphabetic character, 0591, and a three-digit number.