| 
 | 
 | 
 | 
 | 
| 
 
M0591111 
 | 
 
Change 
 | 
 
String1 was converted into string2. 
 | 
 
The token was converted. 
 | 
| 
 
M0591112 
 | 
 
Change 
 | 
 
Bit access of I/O register was converted into macro call. 
 | 
 
Since the bit access method of SFRs differs between the CA78K0R and CC-RL, the method is changed to make access using a macro. 
 | 
| 
 
M0591113 
 | 
 
Change 
 | 
 
'String' has been changed to syntax of CC-RL. 
 | 
 
Since the description format differs between the CA78K0R and CC-RL, the description format is changed to that of the CC-RL. 
 | 
| 
 
M0591121 
 | 
 
Insert 
 | 
 
Inserted macro definition for bit access of I/O register. 
 | 
 
Since the bit access method of SFRs differs between the CA78K0R and CC-RL, the method is changed to make access using a macro. 
 | 
| 
 
M0591122 
 | 
 
Insert 
 | 
 
Inserted #pragma interrupt NO_VECT. 
 | 
 
#pragma interrupt without the vector table specification was generated. 
 | 
| 
 
M0591123 
 | 
 
Insert 
 | 
 
Inserted string. 
 | 
 
A description in accordance with the CC-RL format was added. 
 | 
| 
 
M0591124 
 | 
 
Insert 
 | 
 
Add inline function string for assembly. 
 | 
 
An inline function for assembly was generated. 
 | 
| 
 
M0591125 
 | 
 
Insert 
 | 
 
Inserted #pragma rtos_interrupt NO_VECT. 
 | 
 
#pragma rtos_interrupt without the vector table specification was generated. 
 | 
| 
 
M0591131 
 | 
 
Delete 
 | 
 
String was deleted. 
 | 
 
The description format is not available in the CC-RL. The description was deleted. 
 | 
| 
 
M0591141 
 | 
 
Info 
 | 
 
string1 was converted into string2. 
But that cannot map in RAM. 
 | 
 
Though the section of #pragma section was changed, there is a possibility that the section cannot be allocated. Check the user's manual of the CC-RL. 
 | 
| 
 
M0591142 
 | 
 
Info 
 | 
 
The section can not be converted. Because there is no matched section. 
 | 
 
The section could not be converted because there is no corresponding section in the CC-RL. 
 | 
| 
 
M0591143 
 | 
 
Info 
 | 
 
Delete "AT start address". 
 | 
 
This was deleted because an address cannot be specified by #pragma section in the CC-RL. 
 | 
| 
 
M0591144 
 | 
 
Info 
 | 
 
The MACRO cannot be converted. Because there is no matched macro. 
 | 
 
The macro could not be converted because there is no corresponding macro in the CC-RL. 
 | 
| 
 
M0591145 
 | 
 
Info 
 | 
 
The label detected in the assembly code. Please correct label to appropriate content. 
 | 
 
Only local labels can be written in an assembly-language function in the CC-RL. Modify the label to have suitable contents. 
 |