|
R_DSADC_Channeln_Get_Result_16bit
|
Reads the results of A/D conversion (16 bits; most significant 16 bits of 24-bit resolution).
Remark | The result of A/D conversion by this API function must be read within the maximum pending time of the A/D conversion result register n after A/D conversion end interrupt INTDSAD is generated. |
[Syntax]
#include "r_cg_macrodriver.h"
void R_DSADC_Channeln_Get_Result_16bit ( uint16_t * const buffer );
|
Remark | n is the channel number. |
[Argument(s)]
|
|
|
|
|
|
uint16_t * const buffer;
|
Pointer to area in which to store the results of A/D conversion
|
[Return value]
None.