|
R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start
|
Starts forced output stop function 2 for timer output TKBOn1.
[Syntax]
void R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.