Renesas Electronics
top
OUTPUT FILES
Intel HEX File
3.5
Intel HEX File
This section explains the Intel HEX file.
Previous Topic
Module, section, and symbol information within the library
Next Topic
Structure of the Intel HEX file
Table of Contents
Assemble List File
Link Map File
Link Map File (When Objects Are Combined)
Library List File
Intel HEX File
Structure of the Intel HEX file
Start linear address record
Extended linear address record
Start segment address record
Extended segment address record
Data record
End of file record
Motorola S-record File
Variable/Function Information File