Follow the steps below in the Download Files dialog box to change the download conditions (object information and symbol information) for load module files.
Select a load module file to download in the [Download file list] area.
Current download conditions for the selected load module file are displayed in the [Download file property] area.
Change each items displayed in the property.
|
Specify whether to download the object information from the specified file. |
|||
|
Specify whether to download the symbol information from the specified fileNote 1. |
|||
|
Select whether to generate the information for the Symbol name completion function when downloadingNote 2. |
|||
|
Generates the information for the symbol name completion function. (i.e. uses the symbol name completion function.) |
|||
|
Does not generate the information for the symbol name completion function. (i.e. does not use the symbol name completion function.) |
|||
If the symbol information have not been downloaded, the source level debugging cannot be performed. |
When [Yes] is selected, the time taken for downloading and the memory usage on the host machine will increase. We recommend selecting [No] in this item if you do not intend to use the symbol name completion function. |
Enable all the configuration in this dialog box and change the download conditions.