Specify the type of preferential breakpoint with a single click of the mouse in the Editor panel/Disassemble panel.
Select from the drop-down list below for each use of the breakpoint.
|
Sets hardware breakpoint with priority, by using the Hardware break function. Once set, it is treated as a Hardware Break event (execution system). |
|
|
Sets software breakpoint with priority, by using the Software break function (except for [Simulator]) (default). |
If the number of the set breakpoints of the specified type exceeds the limit settable (see "2.15.7.1 Maximum number of enabled events"), a breakpoint of another type will be used. |
Select whether to terminate the peripheral emulation of timers while stopping the program execution (Peripheral Break).
Select [Yes] to terminate (default: [No]).
This property appears only when the selected microcontroller supports the function that terminates the peripheral emulation of serials (Peripheral Break).
Select whether to terminate the peripheral emulation of serials while stopping the program execution.
Select [Yes] to terminate (default: [No]).
This property appears only when the selected microcontroller supports the open break function.
Select from the following drop-down list whether to use the open break function.
The default value depends on the type of the selected microcontroller.