|
[General - Text Editor] category
|
Use this category to configure general settings relating to the text editor.
Figure A.54 | Option Dialog Box ([General - Text Editor] Category) |
The following items are explained here.
[How to open]
- | From the [Tool] menu, select [Options...]. |
[Description of each area]
Use this area to configure the spacing-related settings in the text editor.
(a) | [Enable auto indentation] |
|
|
Code is intelligently indented depending on the code being typed in the text editor.
E.g. Inside a function or not or coding a loop (default).
|
|
|
Code is not indented depending on the code being typed in the text editor.
|
|
|
When you press the [Tab] key in the text editor, a group of space characters is inserted equal to the width of a tab.
|
|
|
When you press the [Tab] key in the text editor, the tab character is inserted (default).
|
(c) | [Show whitespace marks] |
|
|
Whitespace marks such as space and tab are shown in the text editor.
|
|
|
Whitespace marks such as space and tab are not shown in the text editor (default).
|
(d) | [Enable line highlight for current] |
|
|
Highlights the current line in the text editor.
|
|
|
Does not highlight the current line in the text editor (default).
|
Use this area to configure general settings in the text editor.
(a) | [Enable syntax coloring] |
|
|
Enables the coloring of keywords in the text editor that have supported file-types (default).
|
|
|
No coloring of keywords is displayed in the text editor.
|
(b) | [Enable smart editing] |
|
|
Enables the smart edit function (default).
|
|
|
Disables the smart edit function.
|
(c) | [Enable code outlining] |
This item is only available if the [Enable syntax coloring] check box is selected.
|
|
Enables the code outlining feature in the text editor.
This enables the expansion and collapse of code blocks for file-types that support it (default).
|
|
|
Does not use the code outlining feature in the text editor.
|
(d) | [Enable file encoding auto detection] |
|
|
Enables automatic determination of the encoding when a file is read (default).
|
|
|
Disables automatic determination of the encoding when a file is read.
|
(e) | [Externally modified files] |
This item allows you to specify the action to be taken for source files that are modified externally to the CS+.
|
Prompt to reload the file
|
When a file open in the text editor is modified externally to the CS+, a message dialog box will be displayed which asks you whether you wish to reload the file or not (default).
If you click the [Yes] button on the message dialog box, this will reload the file from disk, losing all current changes to that file in the text editor.
If you click the [No] button on the message dialog box, this will ignore the external changes and any existing modifications to that file in the text editor will remain.
|
|
Always reload the file
|
This will automatically reload the file when it is modified externally.
|
|
Never reload the file
|
This will ignore any externally-modified changes to source files and will not reload the file.
|
(f) | [Default file encoding] |
This option is for the default file encoding that should be used when creating a new file in the Editor panel and automatic determination of encoding is disabled. In addition this encoding is used when the file being opened has a file encoding that cannot be detected or is not supported in the Editor panel currently.
Select the encoding to be set from the drop-down list.
The items of the drop-down list are displayed according to the following sequence.
Note that the same encoding and encoding which are not supported by the current OS will not be displayed.
- | Default encoding of the current OS (default) |
- | Most recently used encodings (maximum 4) |
- | Popular encodings for current locale
e.g. for United States locale it will be: |
- | Western European (Windows) |
- | All other encodings supported by the OS (in alphabetical order) |
Caution 1. | If you wish to select a different encoding in the text editor and save the file, use [Target Save Option...] of the [File] menu for the editing file. Note that [Default file encoding] does not override the setting. |
Caution 2. | If you wish to make an encoding setting specific to building, modify the corresponding property of the build tool listed in the tables below, respectively. Note that [Default file encoding] does not override these settings. |
|
|
|
|
CC-RH
|
[Character encoding] property in the [Character Encoding] category from the [Compile Options] tab or [Individual Compile Options] tab
|
|
[Character encoding] property in the [Character Encoding] category from the [Assemble Options] tab or [Individual Assemble Options] tab
|
|
CC-RX
|
[Character code of an input program] property in the [Source] category from the [Compile Options] tab, [Individual Compile Options(C)] tab, or [Individual Compile Options(C++)] tab
|
|
[Character code of an output assembly-language file] property in the [Object] category from the [Compile Options] tab, [Individual Compile Options(C)] tab, or [Individual Compile Options(C++)] tab
|
|
[Character code of an input program] property in the [Source] category from the [Assemble Options] tab or [Individual Assemble Options] tab
|
|
CC-RL
|
[Character encoding] property in the [Character Encoding] category from the [Compile Options] tab or [Individual Compile Options] tab
|
|
[Character encoding] property in the [Character Encoding] category from the [Assemble Options] tab or [Individual Assemble Options] tab
|
Use this area to configure general settings relating to debugging in the text editor.
(a) | [Enable line highlight for PC] |
|
|
Shows the current PC as a full line highlight in the text editor (default).
|
|
|
Does not show the current PC as a full line highlight in the text editor.
|
(b) | [Enable tool-tip watch] |
|
|
Shows the value of variables in a tool-tip when hovering the mouse over the variable in the text editor (default).
|
|
|
Does not show the value of variables in a tool-tip.
|
(c) | [Enable line highlight for break/coverage] |
|
|
Shows the break and coverage as a full line highlight in the text editor (default).
|
|
|
Does not show the break and coverage as a full line highlight in the text editor.
|
(d) | [Use window recycling] |
|
|
Uses window recycling.
|
|
|
Does not use window recycling (default).
|
Remark | See "CS+ Integrated Development Environment Users Manual: Debug Tool" for details about window recycling. |
|
Initialize Settings
|
Returns all currently displayed setting to their default values.
|
[Function buttons]
|
|
|
|
Initialize All Settings
|
Restores all settings on this dialog box to their default values.
Note, however, that newly added items in the [General - External Tools] category will not be removed.
|
|
OK
|
Applies all setting and closes this dialog box.
|
|
Cancel
|
Ignores the setting and closes this dialog box.
|
|
Apply
|
Applies all setting (does not close this dialog box).
|
|
Help
|
Displays the help of this dialog box.
|