This tab shows the detailed information on a C source file categorized by the following and the configuration can be changed.
Note that this tab takes over the settings of the [Compile Options] tab.
If the settings are changed from the [Compile Options] tab, the properties are displayed in boldface.
This tab is displayed only when [Yes] in the [Set individual compile option] property in the [Build] category from the [Build Settings] tab is selected. |
[Description of each category]
The detailed information on the source is displayed and the configuration can be changed.
|
Specifies the name of the path to the folder that stores the include file. The following placeholders are supported. %ActiveProjectDir%: Replaces with the absolute path of the active project folder. %ActiveProjectName%: Replaces with the active project name. %BuildModeName%: Replaces with the build mode name. %MainProjectDir%: Replaces with the absolute path of the main project folder. %MainProjectName%: Replaces with the main project name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectDir%: Replaces with the absolute path of the project folder. %ProjectName%: Replaces with the project name. %TempDir%: Replaces with the absolute path of the temporary folder. %WinDir%: Replaces with the absolute path of the Windows system folder. The reference point of the path is the project folder. |
||||||
|
Edit by the Path Edit dialog box which appears when clicking the [...] button. For the subproperty, you can use the text box directly enter the text. |
||||||
|
Selects whether to compile using the include path specified in the [Additional include paths] property in the [Source] category from the [Compile Options] tab of the build tool to be used. The include paths are added by the following procedure.
|
||||||
|
Compiles using the include path specified in the property of the build tool to be used. |
||||||
|
Does not use the include path specified in the property of the build tool to be used. |
||||||
|
Specifies include files at the head of compiling units. The following placeholders are supported. %ActiveProjectDir%: Replaces with the absolute path of the active project folder. %ActiveProjectName%: Replaces with the active project name. %BuildModeName%: Replaces with the build mode name. %MainProjectDir%: Replaces with the absolute path of the main project folder. %MainProjectName%: Replaces with the main project name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectDir%: Replaces with the absolute path of the project folder. %ProjectName%: Replaces with the project name. %TempDir%: Replaces with the absolute path of the temporary folder. %WinDir%: Replaces with the absolute path of the Windows system folder. |
||||||
|
Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box. |
||||||
|
Specifies the macro name to be defined. Specify in the format of "macro name=string", with one macro name per line. The "=string" part can be omitted, and in this case, the macro name is assumed to be defined. |
||||||
|
Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can use the text box directly enter the text. |
||||||
|
Specifies invalidates the predefined macro. If multiple macro names are specified, delimit them with a comma (example: __DBL4,__SCHAR). |
||||||
|
Edit by the Specify The Predefined Macro dialog box which appears when clicking the [...] button. |
||||||
|
Specifies whether information level messages are output. This corresponds to the -message and -nomessage options of the compiler. |
||||||
|
Specifies suppresses the number of information-level message. If multiple message numbers are specified, delimit them with a comma (example: 4,200). Also, the range can be set using hyphen (example: 4,200-203,1300). This corresponds to the -nomessage option of the compiler. This property is displayed only when [No(-nomessage)] in the [Enables information-level message output] property is specified. |
||||||
|
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button. |
||||||
|
Changes the warning-level messages to information-level messages |
Selects whether to change the warning-level messages to information-level messages. This corresponds to the -change_message option of the compiler. |
|||||
|
Changes all warning-level messages to the information-level messages. |
||||||
|
Yes(Specifies error number) (-change_message=information=<ErrorNumber>) |
Changes the warning-level messages with the specified error numbers to the information-level messages. |
|||||
|
Does not change the warning-level messages to the information-level messages. |
||||||
|
Specifies error number of warning-level message. If multiple message numbers are specified, delimit them with comma (example: 4,200). Also, the range can be set using hyphen (example: 4,200-203,1300). This corresponds to the -change_message option of the compiler. This property is displayed only when [Yes(Specifies error number) (-change_message=information=<ErrorNumber>)] in the [Changes the warning-level messages to information-level messages] property is specified. |
||||||
|
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button. |
||||||
|
Changes the information-level messages to warning-level messages |
Selects whether to change the information-level messages to warning-level messages. This corresponds to the -change_message option of the compiler. |
|||||
|
Changes all information-level messages to warning-level messages. |
||||||
|
Yes(Specifies error number) (-change_message=warning=<ErrorNumber>) |
Changes the information-level messages with the specified error numbers to warning-level messages. |
|||||
|
Does not change the information-level messages to warning-level messages. |
||||||
|
Specifies error number of information-level message. If multiple message numbers are specified, delimit them with comma (example: 4,200). Also, the range can be set using hyphen (example: 4,200-203,1300). This corresponds to the -change_message option of the compiler. This property is displayed only when [Yes(Specifies error number) (-change_message=warning=<ErrorNumber>)] in the [Changes the information-level messages to warning-level messages] property is specified. |
||||||
|
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button. |
||||||
|
Changes the information-level and warning-level messages to error-level messages |
Selects whether to change the information-level and warning-level messages to error-level messages. This corresponds to the -change_message option of the compiler. |
|||||
|
Changes all information-level and warning-level messages to error-level messages. |
||||||
|
Yes(Specifies error number) (-change_message=error=<ErrorNumber>) |
Changes the information-level and warning-level messages with the specified error numbers to error-level messages. |
|||||
|
Does not change the warning-level messages to information-level messages. |
||||||
|
Specifies error number of information-level and warning-level message. If multiple message numbers are specified, delimit them with comma (example: 4,200). Also, the range can be set using hyphen (example: 4,200-203,1300). This corresponds to the -change_message option of the compiler. This property is displayed only when [Yes(Specifies error number) (-change_message=error=<ErrorNumber>)] in the [Changes the information-level and warning-level messages to error-level messages] property is specified. |
||||||
|
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button. |
||||||
|
Path to the folder that stores a file for inter-file inline expansion |
Specifies path to the folder that stores a file for inter-file inline expansion. The following placeholders are supported. %ActiveProjectDir%: Replaces with the absolute path of the active project folder. %ActiveProjectName%: Replaces with the active project name. %BuildModeName%: Replaces with the build mode name. %MainProjectDir%: Replaces with the absolute path of the main project folder. %MainProjectName%: Replaces with the main project name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectDir%: Replaces with the absolute path of the project folder. %ProjectName%: Replaces with the project name. %TempDir%: Replaces with the absolute path of the temporary folder. %WinDir%: Replaces with the absolute path of the Windows system folder. The reference point of the path is the project folder. This corresponds to the -include option of the compiler. The specified include path is displayed as the subproperty. This property is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or lower or when V2.00.00 or lower is selected in the [Using compiler package version] property. |
|||||
|
Edit by the Path Edit dialog box which appears when clicking the [...] button. For the subproperty, you can use the text box directly enter the text. |
||||||
|
Selects whether to check the compatibility with an existing program. |
||||||
|
Checks the compatibility with the R8C and M16C family C compilers. |
||||||
|
Checks the compatibility with the H8, H8S, and H8SX family C/C++ compilers. |
||||||
|
Checks the compatibility with the SuperH family C/C++ compilers. |
||||||
|
Selects character code of an input program. [Traditional Chinese character (-big5)] and [Simplified Chinese character (-gb2312)] are synchronized with the value of the [Character code of an output assembly-language file] property in the [Object] category. This corresponds to the -euc, -sjis, -latin1, -utf8, -big5 and -gb2312 option of the compiler. option of the compiler. [Traditional Chinese character (-big5)] and [Simplified Chinese character (-gb2312)] are displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or higher or when V2.00.00 or higher is selected in the [Using compiler package version] property. [UTF-8 code (-utf8)] cannot be selected in the following cases.
|
||||||
|
Handles the characters in strings, character constants, and comments by using EUC. |
||||||
|
Handles the characters in strings, character constants, and comments by using SJIS. |
||||||
|
Handles the characters in strings, character constants, and comments by using ISO-Latin1. |
||||||
|
Handles the characters in strings, character constants, and comments by using UTF-8. |
||||||
|
Handles the characters in strings, character constants, and comments by using Traditional Chinese character. |
||||||
|
Handles the characters in strings, character constants, and comments by using Simplified Chinese character. |
||||||
The detailed information on object is displayed and the configuration can be changed.
|
Selects the type of the output file to be generated during a build. |
||||||||
|
Source file after preprocessed(Disables #line output) (-output=prep -noline) |
||||||||
|
Specifies the output destination folder for the output file. The following placeholders are supported. %BuildModeName%: Replaces with the build mode name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectName%: Replaces with the project name. If this is blank, it is assumed that the project folder has been specified. This corresponds to the -output option of the compiler. This property is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or lower or when V2.00.00 or lower is selected in the [Using compiler package version] property. |
||||||||
|
Directly enter in the text box or edit by the Browse For Folder dialog box which appears when clicking the [...] button. |
||||||||
|
Specifies the name of the object module file generated after compilation. The extension other than ".obj" cannot be specified. If the extension is omitted, ".obj" is automatically added. If this is blank, the file name will be the source file name with the extension replaced by ".obj". This corresponds to the -output option of the compiler. This property is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or higher or when V2.00.00 or higher is selected in the [Using compiler package version] property. |
||||||||
|
Selects whether to output debugging information to object module files. This corresponds to the -debug and -nodebug options of the compiler. |
||||||||
|
Does not output debugging information to object module files. |
||||||||
|
Specifies the section name of switch statement branch table area. |
||||||||
|
Allocates uninitialized variables to 4-byte boundary alignment sections |
Selects whether to allocate uninitialized variables to 4-byte boundary alignment sections. |
|||||||
|
Allocates uninitialized variables to 4-byte boundary alignment sections. |
||||||||
|
Does not allocate uninitialized variables to 4-byte boundary alignment sections. |
||||||||
|
Allocates initialized variables to 4-byte boundary alignment sections |
Selects whether to allocate initialized variables to 4-byte boundary alignment sections. |
|||||||
|
Allocates initialized variables to 4-byte boundary alignment sections. |
||||||||
|
Does not allocates initialized variables to 4-byte boundary alignment sections. |
||||||||
|
Allocates const qualified variables to 4-byte boundary alignment sections |
Selects whether to allocate const qualified variables to 4-byte boundary alignment sections. |
|||||||
|
Allocates const qualified variables to 4-byte boundary alignment sections. |
||||||||
|
Does not allocate const qualified variables to 4-byte boundary alignment sections. |
||||||||
|
Allocates switch statement branch tables to 4-byte boundary alignment sections |
Selects whether to allocate switch statement branch tables to 4-byte boundary alignment sections. |
|||||||
|
Allocates switch statement branch tables to 4-byte boundary alignment sections. |
||||||||
|
Does not allocate switch statement branch tables to 4-byte boundary alignment sections. |
||||||||
|
Selects adjustment for instruction in branch. This corresponds to the -noinstalign, -instalign4, and -instalign8 option of the compiler. |
||||||||
|
Aligns instructions at branch destinations to 4-byte boundaries. |
||||||||
|
Execution in 4 bytes(Contains each loop head) (-instalign4=loop) |
Aligns instructions at branch destinations to 4-byte boundaries (Contains head of each loop). |
|||||||
|
Execution in 4 bytes(Contains each inmost loop head) (-instalign4=inmostloop) |
Aligns instructions at branch destinations to 4-byte boundaries (Contains head of each inmost loop). |
|||||||
|
Aligns instructions at branch destinations to 8-byte boundaries. |
||||||||
|
Execution in 8 bytes (Contains each loop head) (-instalign8=loop) |
Aligns instructions at branch destinations to 8-byte boundaries (Contains head of each loop). |
|||||||
|
Execution in 8 bytes (Contains each inmost loop head) (-instalign8=inmostloop) |
Aligns instructions at branch destinations to 8-byte boundaries (Contains head of each inmost loop). |
|||||||
|
Generates divisions and residues with DIV, DIVU, and the FDIV instruction |
Selects whether to generate divisions and residues with DIV, DIVU, and the FDIV instruction. This corresponds to the -nouse_div_inst option of the compiler. |
|||||||
|
Generates code in which DIV, DIVU, or FDIV instructions are used. |
||||||||
|
Generates code in which no DIV, DIVU, or FDIV instructions are used. |
||||||||
|
Selects character code of an output assembly-language file. [Traditional Chinese character (-big5)] and [Simplified Chinese character (-gb2312)] are synchronized with the value of the [Character code of an input program] property in the [Source] category. This corresponds to the -outcode option of the compiler. [Traditional Chinese character (-big5)] and [Simplified Chinese character (-gb2312)] are displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or higher or when V2.00.00 or higher is selected in the [Using compiler package version] property. [UTF-8 code (-outcode=utf8)] cannot be selected in the following cases.
|
||||||||
|
Outputs characters in strings and character constants using EUC. |
||||||||
|
Outputs characters in strings and character constants using SJIS. |
||||||||
|
Outputs characters in strings and character constants using UTF-8. |
||||||||
|
Outputs characters in strings and character constants using Traditional Chinese character. |
||||||||
|
Outputs characters in strings and character constants using Simplified Chinese character. |
||||||||
The detailed information on the quality improvement is displayed and the configuration can be changed.
|
Selects whether to detect the stack smashing. This property is usable only in the Professional Edition. Detection of stack smashing is a feature for writing a value outside the valid stack area before entering a function and checking whether that value is rewritten before exiting the function. Upon detection, the user-defined __stack_chk_fail() function is called. See "CC-RX Compiler User's Manual" about the difference between [Yes(-stack_protector)] and [Yes(All)(-stack_protector_all)]. This corresponds to the -stack_protector and -stack_protector_all options of the ccrx command. This property is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.04.00 or higher or when V2.04.00 or higher is selected in the [Using compiler package version] property. |
||||||
|
Specifies the value to be embedded for detecting the stack smashing. This property is usable only in the Professional Edition. This corresponds to the -stack_protector and -stack_protector_all options of the ccrx command. This property is displayed in the following cases.
|
||||||
The detailed information on list file is displayed and the configuration can be changed.
The detailed information on the optimization is displayed and the configuration can be changed.
|
Partially optimizes the program by automatically allocating variables to registers, integrating the function exit blocks, integrating multiple instructions which can be integrated, etc. |
||||||||
|
Outputs additional information for inter-module optimization |
Selects whether to output additional information for inter-module optimization. At linkage, inter-module optimization is applied to files for which this option has been specified. |
|||||||
|
Outputs additional information for inter-module optimization. |
||||||||
|
Does not outputs additional information for inter-module optimization. |
||||||||
|
This corresponds to the -speed and -size option of the compiler. |
||||||||
|
Selects whether to optimize the loop expansion (for, while, and do-while). |
||||||||
|
Depends on the optimization level and optimization type options |
Depends on the optimization level and optimization type options. |
|||||||
|
Specifies expansion maximum number. This corresponds to the suboption of -loop option of the compiler. This property is displayed only when [Expansion (-loop=<numeric value>)] in the [Loop expansion] property is selected. |
||||||||
|
Selects whether to perform inline expansion automatically. This option corresponds to the -inline and -noinline option of the compiler. |
||||||||
|
Depends on the optimization level and optimization type options |
Depends on the optimization level and optimization type options. |
|||||||
|
Specifies maximum increasing rate of function size. For example, when 100 is specified, inline expansion will be performed until the function size has increased by 100% (size is doubled). This option corresponds to the -inline option of the compiler. This property is displayed only when [Yes (-inline=<numeric value>)] in the [Performs inline expansion automatically] property is selected. |
||||||||
|
Specifies files for inter-file inline expansion. This option is valid only when the inline option or #pragma inline has been specified. The following placeholders are supported. %BuildModeName%: Replaces with the build mode name. %ProjectName%: Replaces with the project name. %MicomToolPath%: Replaces with the absolute path of the product install folder. This option corresponds to the -file_inline option of the compiler. The file name is displayed as the subproperty. This property is displayed only in the following cases.
|
||||||||
|
Click the [...] button to open the Path Edit dialog box. -> Edit by the Add Inline Expansion File dialog box which appears when clicking the [Browse...] button. For the subproperty, you can use the text box directly enter the text. |
||||||||
|
Handles external variables as if they are volatile qualified |
Selects whether to handle all external variables as if they are volatile qualified. This corresponds to the -volatile and -novolatile option of the compiler. |
|||||||
|
Handles all external variables as if they were volatile qualified. |
||||||||
|
Does not handle external variables as if they were volatile qualified. |
||||||||
|
Performs the constant propagation of const qualified external variables |
Selects whether to perform the constant propagation of const qualified external variables. Const qualified variables in a C++ source file cannot be controlled by this option (constant propagation is always performed). This corresponds to the -const_copy and -noconst_copy option of the compiler. |
|||||||
|
Enables constant propagation of const qualified external variables. |
||||||||
|
Disables constant propagation of const qualified external variables. |
||||||||
|
Conversion method of the divisions and residues of integer constants |
Selects conversion method of the divisions and residues of integer constants. This corresponds to the -const_div and -noconst_div option of the compiler. |
|||||||
|
Performs constant division (residue) by an instruction sequence using multiplication. |
||||||||
|
Performs constant division (residue) by an instruction sequence using division. |
||||||||
|
Performs instruction expansion of several library functions (-library=intrinsic) |
Performs instruction expansion for abs(), fabsf(), and library functions which can use string manipulation instructions. |
|||||||
|
Divides the optimizing ranges into many sections before compilation |
Selects whether to divide the optimizing ranges of the large-size function into many sections This corresponds to the -scope and -noscope option of the compiler. |
|||||||
|
Divides the optimizing ranges of the large-size function into many sections before compilation. |
||||||||
|
Schedules the instruction taking into consideration pipeline processing |
Selects whether to schedule the instruction taking into consideration pipeline processing. This corresponds to the -schedule and -noschedule option of the compiler. |
|||||||
|
Schedules instructions taking into consideration pipeline processing. |
||||||||
|
Selects whether to optimize accesses to external variables. This corresponds to the -nomap, -smap and -map option of the compiler. |
||||||||
|
Optimizes accesses to external variables which are defined in the file to be compiled. |
||||||||
|
Specifies the level of inter-module optimization (such as function merging). This corresponds to the -whole_program, -merge_files, and -ip_optimize option of the compiler. This property is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.00.00 or higher or when V2.00.00 or higher is selected in the [Using compiler package version] property. |
||||||||
|
Converts floating-point constant division into multiplication |
Selects whether to convert floating-point constant division into multiplication of the corresponding reciprocals as constants. |
|||||||
|
Converts floating-point constant division into multiplication. |
||||||||
|
Does not convert floating-point constant division into multiplication. |
||||||||
|
Allocates preferentially the variables with register storage class specification to registers |
Selects whether to allocate preferentially the variables with register storage class specification to registers. This corresponds to the -enable_register option of the compiler. This property is displayed only in the following cases.
|
|||||||
|
Allocates preferentially the variables with register storage class specification to registers. |
||||||||
|
Does not allocate preferentially the variables with register storage class specification to registers. |
||||||||
|
Omits a check of the range for conversion between the floating type and unsigned integer type |
Selects whether to omit a check of the range for conversion between the floating type and unsigned integer type. When "Yes" is specified, code performance of the relevant type conversion processing is improved. The conversion result may, however, differ from C/C++ language specifications, so take care on this point. This corresponds to the -simple_float_conv option of the compiler. |
|||||||
|
Omits part of the type conversion processing for the floating type. |
||||||||
|
Does not omit part of the type conversion processing for the floating type. |
||||||||
|
Performs optimization considering the type of the data indicated by the pointer |
Selects whether to perform optimization considering the type of the data indicated by the pointer. Although the performance of object code is generally better than when -alias=noansi is specified, the results of execution may differ according to whether -alias=ansi or alias=noansi is specified. |
|||||||
|
Performs optimization considering the type of the data indicated by the pointer. |
||||||||
|
Does not perform optimization considering the type of the data indicated by the pointer. |
||||||||
|
Optimizes modification of the operation order of a floating-point expression |
Selects whether to optimize modification of the operation order of a floating-point expression. Specifying the -float_order option generally improves the object performance compared to when not specifying it. However, the accuracy of operations may differ from that when -float_order is not specified. This corresponds to the -float_order option of the compiler. This property is valid only when [2 (-optimize=2)] or [Max (-optimize=max)] in the [Optimization level] property is specified. |
|||||||
|
Optimizes modification of the operation order in a floating-point expression. |
||||||||
|
Does not optimize modification of the operation order in a floating-point expression. |
||||||||
The detailed information on the output file check is displayed and the configuration can be changed.
Select whether to output the assembly source file of the compile result for the C source.
This corresponds to the -output=src option of the compiler.
The detailed information on the MISRA-C rules check is displayed and the configuration can be changed.
20XX in the following table corresponds to 2012 or 2004 in particular.
|
Selects the MISRA-C specification. This property is usable only in the Professional Edition. This property is displayed when [Always latest version which was installed] in the [Using compiler package version] property in the [Version Select] category from the [Common Options] tab is selected and the latest version is V2.04.00 or higher or when V2.04.00 or higher is selected in the [Using compiler package version] property. |
||||
|
Settings for MISRA-C 2012 are made in the subsequent properties. |
||||
|
Settings for MISRA-C 2004 are made in the subsequent properties. |
||||
|
Selects to apply MISRA C rule. This property is usable only in the Professional Edition. This option corresponds to the -misra20XX option of the compiler. |
||||
|
Checks the source code against all of the rules that are supported. |
||||
|
Checks the source code against the rules with the selected numbers. |
||||
|
Checks the source code against the rules other than those with the selected numbers. |
||||
|
Apply rules that are classified as "required" (-misra20XX=required) |
Checks the source code against the rules of the "required" type. |
|||
|
Apply rules that are classified as "required" and specified rule number (-misra20XX=required_add) |
Checks the source code against the rules of the "required" type and the rules with the selected numbers. |
|||
|
Ignore specified rule number from rules that are classified as "required" (-misra20XX=required_remove) |
Checks the source code against the rules other than those with the selected numbers among the rules of the "required" type. |
|||
|
Apply rules that are described in the specified file (-misra20XX=<file name>) |
Checks the source code against the rules with the numbers written in the specified file. |
|||
|
Specifies Rule number description file(misra20XX rule file). This property is usable only in the Professional Edition. The following placeholders are supported. %BuildModeName%: Replaces with the build mode name. %ProjectName%: Replaces with the project name. %MicomToolPath%: Replaces with the absolute path of the product install folder. This option corresponds to the -misra20XX option of the compiler. This property is displayed only when [Apply rules that are described in the specified file (-misra20XX=<file name>)] in the [Apply rule] property is selected. |
||||
|
Directly enter to the text box or edit by the Specify Misra20XX Rule File dialog box which appears when clicking the [...] button. |
||||
|
This property is usable only in the Professional Edition. One or more rule numbers always in decimal must be specified. This option corresponds to the -misra20XX option of the compiler. This property is displayed only when [Apply specified rule number (-misra20XX=apply)] in the [Apply rule] property is selected. |
||||
|
Directly enter to the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button. |
||||
|
Specifies the exclusion rule number. This property is usable only in the Professional Edition. One or more rule numbers always in decimal must be specified. This option corresponds to the -misra20XX option of the compiler. This property is displayed only when [Ignore specified rule number(-misra20XX=ignore)] in the [Apply rule] property is selected. |
||||
|
Directly enter to the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button. |
||||
|
Specifies the check rule number besides required rule. This property is usable only in the Professional Edition. One or more rule numbers always in decimal must be specified. This option corresponds to the -misra20XX option of the compiler. This property is displayed only when [Apply rules that are classified as "required" and specified rule number (-misra20XX=required_add)] in the [Apply rule] property is selected. |
||||
|
Directly enter to the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button. |
||||
|
Specifies the exclusion rule number from required rule. This property is usable only in the Professional Edition. One or more rule numbers always in decimal must be specified. This option corresponds to the -misra20XX option of the compiler. This property is displayed only when [Ignore specified rule number from rules that are classified as "required" (-misra20XX=required_remove)] in the [Apply rule] property is selected. |
||||
|
Directly enter to the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button. |
||||
|
Specifies rule check exclusion file. This property is usable only in the Professional Edition. The following placeholders are supported. %BuildModeName%: Replaces with the build mode name. %ProjectName%: Replaces with the project name. %MicomToolPath%: Replaces with the absolute path of the product install folder. This option corresponds to the -ignore_files_misra option of the compiler. This option is not display when [Not apply rule] in the [Apply rule] property has been specified. |
||||
|
Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box. |
||||
|
Outputs message of The the enhanced key word and extended specifications |
Selects whether to output message of The the enhanced key word and extended specifications. This property is usable only in the Professional Edition. This option corresponds to the -check_language_extension option. This option is not display when [Not apply rule] in the [Apply rule] property has been specified. |
|||
|
Enables complete checking against the MISRA-C rules for parts of the code where it would otherwise be suppressed due to individual extensions from the C/C++ language specification. |
||||
|
Disables complete checking against the MISRA-C rules for parts of the code where it would otherwise be suppressed due to individual extensions from the C/C++ language specification. |
||||
Other detailed information on compilation is displayed and the configuration can be changed.