Below chart describes contents of Variable List Panel. For the details, refer to help.
"Static" information is described after build. "Dynamic" information is described after connecting the debug tool.
|
Description |
Overview |
Static/Dynamic |
|
Variable Name |
Name of the variables defined/referenced in C source |
Static |
|
File Name |
File name of C source file where the variable is defined |
Static |
|
File Path |
Name of the function where the variable is defined |
Static |
|
Import |
Source of the variable information |
Static |
|
Attribute |
Variable's symbol attributes/symbol-modifier attributes |
Static |
|
Type |
Type of the variable |
Static |
|
Members |
Members of the structure/union |
Static |
|
Address |
Variable's allocated address |
Static |
|
Size |
Size of the variables |
Static |
|
Reference Count |
Number of times the variable is referenced in the program |
Static |
|
Read Count |
Number of times the variable was read |
Dynamic |
|
Write Count |
Number of times the variable was written |
Dynamic |
|
Read/Write Count |
Number of times the variable was read/write |
Dynamic |
|
Minimum Value |
Minimum value stored in variables |
Dynamic |
|
Maximum Value |
Maximum value stored in variables |
Dynamic |
|
Data Coverage |
Data coverage ratio of the variable |
Dynamic |
|
Total |
Total of above item in the target file |
- |