Main window


This is the first window to open when CS+ is launched.

In this window. you can open panels for the analysis tool.

Figure A.1

Main Window

 

The following items are explained here.

[How to open]

-

From the Windows [start] menu, select [All Programs] >> [Renesas Electronics CS+] >> [CS+ for CC].

Remark

In Windows 8 or Windows 8.1, select [CS+ for CC (RL78,RX,RH850)] on the start screen.
In Windows 10, select Windows [Start] >> [All apps] >> [Renesas Electronics CS+] >> [CS+ for CC (RL78,RX,RH850)].

[Description of each area]

(1)

Menubar

(a)

[View]

The [View] menu for the analysis tool provides the following items and functions (default).

Output

Opens the Output panel.

Program Analyzer

The following cascade menus are displayed to open panels for the analysis tool.

 

Function List

Opens the Function List panel.

Variable List

Opens the Variable List panel.

Analysis Chart

Opens the Analysis Chart panel.

Call Graph

Opens the Call Graph panel.

Class/Member

Opens the Class/Member panel.

(2)

Toolbar

The toolbar for the analysis tool provides the following items and functions (default).

 

Opens the Function List panel.

The function of this item is the same as that of [Function List] in the [View] menu.

 

Opens the Variable List panel.

The function of this item is the same as that of [Variable List] in the [View] menu.

 

 

Opens the Analysis Chart panel.

The function of this item is the same as that of [Analysis Chart] in the [View] menu.

 

Opens the Call Graph panel.

The function of this item is the same as that of [Call Graph] in the [View] menu.

 

Opens the Class/Member panel.

The function of this item is the same as that of [Class/Member] in the [View] menu.

(3)

Panel display area

This area consists of multiple panels, each dedicated to a different purpose.

See the following sections for details on a panel used by the analysis tool.