Select Modules Which Are Output in Files dialog box


This dialog box is used to set modules which are output to the I/O header file.

Figure A.24

Select Modules Which Are Output in Files Dialog Box

 

The following items are explained here.

[How to open]

-

On the Property panel, select the following property, and then click the [...] button.

-

From the [I/O Header File Generation Options] tab, [Modules which are defined in device file] in the [I/O Header File] category

[Description of each area]

(1)

Area for specifying module name/file name

This area displays a list of the names of modules defined in the device file and the names of the I/O header files to which the modules are output.

(a)

[Module Name]

This area displays the names of modules which are defined in the device file.

If any of the check boxes is selected, the relevant module is output to the I/O header file shown under [File Name].

The check boxes are selected by default.

(b)

[File Name]

This area displays the names of the I/O header files to which the modules are output.

You can also directly enter a desired file name to change the I/O header file to which the module is output.

The default file name is iodefine.h.

(c)

[Select all/Release all]

This check box is used to select or deselect all of the check boxes under [Module Name].

If this check box is selected, check boxes under [Module Name] will all be selected.

If this check box is deselected, selection of the check boxes under [Module Name] will all be cleared.

[Function buttons]

Button

Function

OK

Closes this dialog box and calls the settings to reflect them in the previous properties.

Initialize

Sets all check boxes under [Module Name] and [File Name] settings to their default values.

Cancel

Cancels the settings and closes this dialog box.

Help

Displays the help of this dialog box.