2.5 Set Assemble Options

To set options for the assemble phase, select the Build tool node on the project tree and select the [Assemble Options] tab on the Property panel.

You can set the various assemble options by setting the necessary properties in this tab.

Figure 2.29

Property Panel: [Assemble Options] Tab

 

Remark

Often used options have been gathered under the [Frequently Used Options(for Assemble)] category on the [Common Options] tab.

Caution

This tab is displayed only when [No] in the [Build simultaneously] property in the [Build Method] category from the [Common Options] tab is selected.