This dialog box is used to set an address when adding or modifying a section.
The following items are explained here.
On the Section Settings dialog box, select an address in the address-section area, and then click the [Add...] or [Modify...] button. |
Specify the start address of the section.
Directly enter the address in the text box or select from the
button.
The range that can be specified for the value is 0 to FFFFF (hexadecimal number) (default: 0).
Closes this dialog box and adds the specified address to an appropriate location in the address-section area in the Section Settings dialog box (the section column remains empty).
Closes this dialog box and moves the section group (an address and the sections allocated to the address) to an appropriate location in the address-section area in the Section Settings dialog box. |
|||||