Select the build tool node on the project tree and select the [Hex Output Options] tab on the Property panel.
The setting of the hex file output range is made with the [Division output file] property in the [Output File] category.
If you click the [...] button, the Text Edit dialog box will open.
Specify the division output file name in [Text] in the format of "file name=start address-end address" (start address, end address: The start address and end address of the output range) or "file name=section name" (section name: The name of the output section), with one file name per line.
If multiple section names are specified, delimit them with a colon as in "file name=section name:section name".
Specify the start address and end address in hexadecimal.
You can specify up to 259 characters per line, up to 65535 lines.
If you click the [OK] button, the entered division output file names are displayed as subproperties.
To change the division output file names, you can use the [...] button or enter them directly in the text box of the subproperty.
Set the method for filling the vacant area in the output range.
Select [Yes(Random)(-SPace=Random)] in the [Fill unused areas in the output ranges with the value] property in the [Hex Format] category.
Select [Yes(Specification value)(-SPace=<Numerical value>)] in the [Fill unused areas in the output ranges with the value] property in the [Hex Format] category. The [Output padding data] property will be displayed.
[Fill unused areas in the output ranges with the value] and [Output padding data] Property |
Enter the fill value for the vacant area directly in the text box.
The range that can be specified for the value is 00 to FFFFFFFF (hexadecimal number).