R_CGC_Create_UserInit


Performs user-define initialization relating to the clock generator (include reset function, on-chip debug function, etc.).

Remark

This API function is called as the R_CGC_Create callback routine.

Syntax

void    R_CGC_Create_UserInit ( void );

Argument(s)

None.

Return value

None.