Renesas Electronics
R_DFE_Set_SoftwareData
Sets the data to be processed.in a target filter.
Syntax
void R_DFE_Set_SoftwareData ( uint8_t tag, int16_t const data );
Argument(s)
I/O
Description
I
uint8_t tag;
Set the same value as the channel tag
int16_t const data;
Software input data
Return value
None.