R_PICn_Timer_SyncStart


Generates start triggers of the timers for which simultaneous start is enabled.

Syntax

void    R_PICn_Timer_SyncStart ( void );

Remark

n is the unit number.

Argument(s)

None.

Return value

None.