3.2.11  
Window Watchdog Timer
 
Below is a list of API functions output by the Code Generator for window watchdog timer use.
| 
Table 3.11 | API Functions: [Window watchdog timer] | 
|  |  | 
| 
R_WDTm_Create | 
Performs initialization necessary to control the watchdog timer functions. | 
| 
R_WDTm_Create_UserInit | 
Performs user-defined initialization relating to the watchdog timer functions. | 
| 
r_wdtm_interrupt | 
Performs processing in response to the interval interrupt. | 
| 
R_WDTm_Restart | 
Clears the watchdog timer counter and resumes counting. |