r_bup_interrupt


Performs processing in response to the power switching detection interrupt INTVBAT.

Remark

This API function is called as the interrupt process corresponding to the power switching detection interrupt INTVBAT.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_bup_interrupt ( void );

 

CC-RL Compiler

static  void  __near r_bup_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.