Performs processing in response to the comparator interrupt INTCMPn.
| 
Remark | This API function is called as the interrupt process corresponding to the comparator interrupt INTCMPn. | 
[Syntax]
CA78K0R Compiler
| __interrupt static  void    r_compn_interrupt ( void ); | 
 
CC-RL Compiler
| static  void  __near r_compn_interrupt ( void ); | 
| 
Remark | n is the channel number. | 
[Argument(s)]
None.
[Return value]
None.