Configures the operation mode of data operation circuit.
[Syntax]
#include r_cg_macrodriver.h
#include r_cg_doc.h
MD_STATUS R_DOC_SetMode ( doc_mode_t mode, uint16_t value);
|
[Argument(s)]
|
|
|
|
|
|
doc_mode_t mode;
|
Operation mode of data operation circuit
ADDTION: Data addition mode
SUBTRACTION: Data subtraction mode
COMPARE_MATCH: Data comparison mode
(Detection Condition: Data match is detected)
COMPARE_MISMATCH: Data subtraction mode
(Detection Condition: Data mismatch is detected)
|
|
|
uint16_t value;
|
Data addition and data subtraction Results of operations
Data comparison 16-bit data for use as a reference
|
[Return value]
|
|
|
|
MD_OK
|
Normal completion
|
|
MD_ARGERROR
|
Invalid argument specification
|