r_fmc_interrupt


Performs processing in response to the end of frequency measurement interrupt INTFM.

Remark

This API function is called as the interrupt process corresponding to the end of frequency measurement interrupt INTFM.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_fmc_interrupt ( void );

 

CC-RL Compiler

static  void  __near r_fmc_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.