Renesas Electronics
r_iican_callback_slave_receiveend
Performs processing in response to the IICA slave reception end interrupt INTIICAn.
Remark
This API function is called as the callback routine of interrupt process r_iican_interrupt corresponding to the IICA slave reception end interrupt INTIICAn.
[Syntax]
static void r_iican_callback_slave_receiveend ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]