Performs processing in response to the external maskable interrupt INTRTCICn.
Remark | This API function is called as the interrupt process corresponding to the external maskable interrupt INTRTCICn. |
[Syntax]
CA78K0R Compiler
__interrupt static void r_intrtcicn_interrupt ( void );
|
CC-RL Compiler
static void __near r_intrtcicn_interrupt ( void );
|
Remark | n is the interrupt factor number. |
[Argument(s)]
None.
[Return value]
None.