r_lvd_vrtcinterrupt


Performs processing in response to the voltage detection of VRTC pin interrupt INTLVDVRTC.

Remark

This API function is called as the interrupt process corresponding to the voltage detection of VRTC pin interrupt INTLVDVRTC.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_lvd_vrtcinterrup ( void );

 

CC-RL Compiler

static  void  __near r_lvd_vrtcinterrup ( void );

[Argument(s)]

None.

[Return value]

None.