Operates the signed multiply.
[Syntax]
#include r_cg_macrodriver.h
#include r_cg_mac32bit.h
void R_MAC32Bit_MULSigned(int32_t data_a, int32_t data_b, mac32bit_int64_t * buffer_64bit);
|
[Argument(s)]
|
|
|
|
|
|
int32_t data_a
|
Multiplicand
|
|
|
int32_t data_b
|
Multiplier
|
|
|
mac32bit_int64_t
* buffer_64bit
|
Multiplier result
|
Remark Below is an example of the structure mac32bit_int64_t for the multiplier result.
typedef struct
{
int16_t low_low;
int16_t low_high;
int16_t high_low;
int16_t high_high;
} mac32bit_int64_t;
|
[Return value]
None.