| 
 R_RTC_Set_CalendarAlarmOn 
 | 
Starts the alarm interrupt function.(in the case of the calendar mode setting)
[Syntax]
#include    "r_cg_macrodriver.h" 
#include    "r_cg_rtc.h" 
void    R_RTC_Set_CalendarAlarmOn ( uint8_t enb_set ); 
 | 
 
[Argument(s)]
 
| 
 | 
 | 
 | 
| 
 | 
uint8_t enb_set; 
 | 
 
Alarm enable 
 | 
Remark  | Below is shown the structure enb_set.  | 
 
[Return value]
None.