Halts the clock supplied to the temperature sensor.
Remark  | Calling this API function changes the temperature sensor to reset status. 
For this reason, writes to the control registers after this API function is called are ignored.  | 
 
[Syntax]
void    R_TMPS_Set_PowerOff ( void ); 
 | 
 
[Argument(s)]
None.
[Return value]
None.