Renesas Electronics
R_TMRDn_Create_UserInit
Performs user-defined initialization relating to the 16-bit timer RDn.
Remark
This API function is called as the R_TMR_RDn_Create callback routine.
[Syntax]
void R_TMRDn_Create_UserInit ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]