R_TMR_RJ0_Set_PowerOff


Halts the clock supplied to the 16-bit timer RJ0.

Remark

Calling this API function changes the 16-bit timer RJ0 to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

[Syntax]

void    R_TMR_RJ0_Set_PowerOff ( void );

[Argument(s)]

None.

[Return value]

None.