Performs processing in response to the LIN-UART reception status interrupt INTLS.
Remark | This API function is called as the callback routine of interrupt process r_uartfn_interrupt_error corresponding to the LIN-UART reception status interrupt INTLS. |
[Syntax]
static void r_uartfn_callback_error ( uint8_t err_type );
|
Remark | n is the channel number. |
[Argument(s)]
|
|
|
|
|
|
uint8_t err_type;
|
Trigger for LIN-UART reception status interrupt
00000xx1B: Overrun error
00000x1xB: Parity error
000001xxB: Framing error
|
[Return value]
None.