Performs processing in response to the timer interrupt.
Remark | This API function is called as the interrupt process corresponding to the timer interrupt. |
[Syntax]
CA78K0R Compiler
__interrupt static void r_wutm_interrupt ( void );
|
CC-RL Compiler
static void __near r_wutm_interrupt ( void );
|
[Argument(s)]
None.
[Return value]
None.