r_cgc_oscillation_stop_interrupt
|
Performs processing in response to the oscillation stop detection interrupt.
Remark | This API function is called to run interrupt processing for the oscillation stop detection interrupt, which is generated when the clock generation circuit detects oscillation by the main clock having stopped. |
[Syntax]
static void r_cgc_oscillation_stop_interrupt ( void );
|
[Argument(s)]
None.
[Return value]
None.