R_GPTn_HardwareStart


Allows detection of GPT interrupts.

Remark

This API function enables GPT interrupts when starting timer count by the hardware trigger.

[Syntax]

void    R_GPTn_HardwareStart ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.