Issues the start condition and causes a transfer error and an event generation interrupt (EEI).
This API function is called as the internal function of R_RIICn_Master_Send and R_RIICn_Master_Receive. |
r_riicn_error_interrupt is called in response to calling of this API function. |