R_RTC_Set_BinaryCounterValue


Sets the value of the binary counter.

[Syntax]

#include    "r_cg_macrodriver.h"
void    R_RTC_Set_BinaryCounterValue ( uint32_t counter_write_val );

[Argument(s)]

I/O

Argument

Description

I

uint32_t  counter_write_val;

The value of the binary counter

[Return value]

None.