Renesas Electronics
r_scifan_callback_receiveend
Performs processing in response to the transmit-end interrupts.
Remark
This API function is called as the r_scifan_txif_interrupt callback routine.
[Syntax]
static void r_scifan_callback_receiveend ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]