1.2 Features

The Code Generator has the following features.

(1)

Code generating function

The Code Generator can output not only device driver programs in accordance with the information configured using the GUI, but also a build environment such as sample programs containing main functions and link directive files.

(2)

Reporting function

You can output configured information using the Code Generator as files in various formats for use as design documents.

(3)

Renaming function

The user can change default names assigned to the files output by the Code Generator and the API functions contained in the source code.