Project Tree panel


This panel displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

Figure A.2

Project Tree Panel

 

The following items are explained here.

[How to open]

-

From the [View] menu, select [Project Tree].

[Description of each area]

(1)

Project tree area

This area displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

(a)

Code Generator (Design Tool)

The sub-nodes of this node are [Peripheral Functions] and [Code Preview].

<1>

[Peripheral Functions]

The sub-node of this node is the peripheral function node for the peripheral functions (clock generator, port functions, etc.) supported by the target device.

Peripheral function node

Double-click on a peripheral function node or press the [Enter] key after selecting a peripheral function node to open the Peripheral Functions panel, which is used to make settings for control of the corresponding peripheral function.

 

Icons that are displayed immediately to the left of each peripheral function node have the meanings listed below.

 

Operation in the corresponding Peripheral Functions panel has been carried out.

 

Operation in the corresponding Peripheral Functions panel has not been carried out.

,

The problem occurs on the settings became the manipulation to the other peripheral function node influences.

 

<2>

[Code Preview]

The sub-node of this node is the peripheral function node for the peripheral functions (clock generator, port functions, etc.) supported by the target device.

Peripheral function node

Double-click on a source code node/API function node in the level of the hierarchy below this node or select a source code node/API function node and press the [Enter] key to open the Code Preview panel, which is used to confirm that the source code corresponds to the settings in the Peripheral Functions panel.

 

Icons that are displayed immediately to the left of each peripheral function node have the meanings listed below.

 

Operation in the corresponding Peripheral Functions panel has been carried out.

 

Operation in the corresponding Peripheral Functions panel has not been carried out.

[Context menu]

Return to Reset Value

The default settings of the selected node are restored.

Property

Opens the Property panel corresponding to the selected node.