20.20 Alarm Handler Information (alarm_handl[])
Here, each alarm handler is defined.
Parentheses < >show the user input part.
- Description
Define the alarm handler ID number.
- Definition format
Numeric value
- Definition range
From 1 to 255
- When omitting
The cfg600px assigns the ID number automatically.
- Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
#define <ID name> <ID number>
- Definition format
Symbol
- When omitting
Cannot be omitted.
3 ) Alarm handler entry address (
entry_address)
- Description
Define the starting function of the alarm handler.
- Definition format
Symbol
- When omitting
Cannot be omitted.
4 ) Extended information (
exinf)
- Description
Define the extended information of the alarm handler.
- Definition format
Numeric value
- Definition range
From 0 to 0xFFFFFFFF
- When omitting
The set value in the default system configuration file (factory setting: 0) applied.
- Note
The extended information is passed to the alarm handler.