-
prcv_mbx
iprcv_mbx
-
Receive from mailbox (polling).
ER prcv_mbx (ID mbxid, T_MSG **ppk_msg);
ER iprcv_mbx (ID mbxid, T_MSG **ppk_msg);
|
|
|
|
|
|
ID mbxid;
|
ID number of the mailbox from which a message is received.
|
|
|
T_MSG **ppk_msg;
|
Start address of the message packet received from the mailbox.
|
typedef struct t_msg {
struct t_msg *msgnext; /*Reserved for future use*/
} T_MSG;
|
[Message packet: T_MSG_PRI]
typedef struct t_msg_pri {
struct t_msg msgque; /*Reserved for future use*/
PRI msgpri; /*Message priority*/
} T_MSG_PRI;
|
This service call receives a message from the mailbox specified by parameter
mbxid, and stores its start address in the area specified by parameter
ppk_msg.
If the message could not be received from the target mailbox (no messages were queued in the wait queue) when this service call is issued, message reception processing is not executed but "E_TMOUT" is returned.
Note 1 If no message could be received from the target mailbox (no messages were queued to the wait queue) when this service call is issued, the contents in the area specified by parameter
ppk_msg become undefined.
|
|
|
|
|
|
|
|
|
|
|
- mbxid > Maximum ID number
|
|
|
|
- This service call was issued in the CPU locked state.
|
|
|
|
- Specified mailbox is not registered.
|
|
|
|
- No message exists in the target mailbox.
|