-g


This option outputs information for source debugging.

[Specification format]

-g

 

-

Interpretation when omitted

Information for source debugging will not be output.

[Detailed description]

-

This option outputs information for source debugging to the output file.

-

Source debugging can be performed by specifying this option.

-

If this option and an optimization option are specified at the same time, the ease of debugging could be affected.

[Example of use]

-

To output information for source debugging to the output file, describe as:

>ccrh -g -Xcommon=rh850 main.c