This option enables the source-code checking of the MISRA-C:2004 or MISRA-C:2012 rules, which are partially suppressed by the extended language specifications.
The source-code checking of the MISRA-C:2004 rules or MISRA-C:2012 rules is disabled, which are partially suppressed by the extended language specifications.
This option enables the source-code checking of the MISRA-C:2004 or MISRA-C:2012 rules in the following cases where they are suppressed by the unique language specifications extended from the C language standard. |
When the function has no prototype declaration (MISRA-C:2004 rule 8.1, MISRA-C:2012 rule 8.4) and #pragma interrupt is specified for it. |
This option is valid only when the -Xmisra2004 option or -Xmisra2012 option is specified. |
To enable the source-code checking of the MISRA-C:2004 rules, which are partially suppressed by the extended language specifications, describe as: |