This option specifies that an object file common to the various devices is generated.
However, an error will not occur if the -V or -h option is specified.
When this option is specified, only instructions are used in the instruction set architecture of the target, and common magic number series that supports the instruction set architecture is embed into the object file. |
The item that can be specified as series is shown below. |
|
It is possible to link to the model with the V850E3v5 instruction set architecture, which is specified as a target device. |
|
To embed the magic number common to models with the instruction set architectures superior to V850E3V5 into the object file to be generated, describe as: |