This option specifies the input binary file.
[Specification format]
-Binary=file(section[:alignment][/attribute][,symbol])[,file(section[:alignment][/attribute][,symbol])]...
|
- | Interpretation when omitted |
None
[Detailed description]
- | This option specifies input binary file file.
If multiple files are specified, delimit them with a comma (,).
|
- | If the extension is omitted from the input file specification, it is assumed that ".bin" has been specified. |
- | Input binary data is allocated as the data of specified section section.
Specify the section address by the -start option.
An error will occur if section is omitted.
|
- | When symbol symbol is specified, it can be linked as a defined symbol.
For a variable name referenced by a C program, add "_" at the head of the reference name in the program.
|
- | The section specified by this option can have its section attribute and number of alignment specified. |
- | CODE or DATA can be specified as section attribute attribute.
If attribute is omitted, the write, read, and execute attributes will be all valid by default.
|
- | The value that can be specified for number of alignment alignment is a power of 2 (1, 2, 4, 8, 16, or 32).
Other value cannot be specified.
If alignment is omitted, "1" will be valid by default.
|
[Example of use]
- | b.bin is allocated from 0x200 as the D1bin section.
c.bin is allocated after D1bin as the D2bin section (with the number of alignment = 4).
The c.bin data is linked as defined symbol "_datab".
To perform the above operations, describe as:
|
>rlink a.obj -start=D*/200 -binary=b.bin(D1bin),c.bin(D2bin:4,_datab)
|
[Remark]
- | If the -form={object|library} option or -strip option is specified, this option will be invalid. |
- | If input object file is not specified, this option cannot be specified. |